Technical FAQs

Ask a Question

Unable to open Unity Pro application, getting error" Object Store internal error......."

Symptom: Unable to open Unity Pro application, getting error "Object Store internal error......." see attachment.

Reason: This issue comes due to non compatibility of Unity Pro with Windows 8, 8.1 & 10.

Solution: Run the Unity Pro in Windows 7 compatibility mode. Right click on the Unity Pro icon, select Compatibility tab, Check the "compatibility mode"  & select Windows 7 from the drop-down menu. Click OK to close the dialog box.
Was this helpful?
What can we do to improve the information ?