Technical FAQs

Ask a Question

Is Micrologic of Masterpact NT/NW incomplaince with EMC directive of IEC?

The Masterpact NT/NW Micrologic conform to Class A EMC environment category as per IEC60947-2 standard.

Pl find attached herewith the EMC certificate.
Was this helpful?
What can we do to improve the information ?