Technical FAQs

Ask a Question

Can we change the trip units of Compact NSX MCCB?

Yes, it is possible to change the trip units in NSX breakers. The only ones for which is not allowed are the types R, HB1, HB2.
Was this helpful?
What can we do to improve the information ?