Technical FAQs

Ask a Question

What is the ambient and storage temperature range for Varset.

Below are the details on temperature ranges for Varset:

a) Ambient Temperature:

-maximum temperature: 40 °C
-average temperature over a 24 hour period: 35 °C
-average temperature over a 1 year period: 25 °C
-minimum temperature: -5 °C

b) Storage: -20 °C to +45 °C.

Was this helpful?
What can we do to improve the information ?