Technical FAQs

Ask a Question

What is the Maximum permissible over current(with thermal protection included) for Varset range.

Below are the details for Maximum permissible over current for Varset:

- 1.43 In for low polluted network.
- 1.31 In for polluted network with 4.2 tuning factor.
- 1.19 In for polluted network with 3.8 tuning factor.
Was this helpful?
What can we do to improve the information ?