Technical FAQs

Ask a Question

Whether the output contacts of Varplus Logic VL used to close the contactor of the capacitor is a permanent latched type or pulse type.


The output contacts of Varplus Logic VL  are permanent latched type.
Was this helpful?
What can we do to improve the information ?