Technical FAQs

Ask a Question

Use of Front port of MCS025 Module of Sepam

Refer the attached Image of front face of MCS025 Module.
The Front port of MCS025 is not meant to use, you should not use it or connect it using any cables. Yes it resembles like the front port of Sepam Base module but not to use for any purpose. 
To set the MCS025 we should use the front port of the Sepam base module only. 

Was this helpful?
What can we do to improve the information ?