Technical FAQs

Ask a Question

Do ION7650 communicate on Modbus TCPIP and IEC61850 protocol at the same time.

Yes ION7650 communicates on IEC61850 & Modbus TCP/IP communication at the same time.
Was this helpful?
What can we do to improve the information ?