Technical FAQs

Ask a Question

Front communication port user interface

The front communication port is provided by a 9-pin female D-type connector located under
the bottom hinged cover. It provides EIA(RS)232 serial data communication and is intended
for use with a PC locally to the relay (up to 15m distance).
Please refer the Attached file.
Was this helpful?
What can we do to improve the information ?