Technical FAQs

Ask a Question

What is the command to open/close Kernel (using a button) in Vijeo Citect Runtime.

The command to call/operate Kernel in Citect Runtime is DspKernel().

- To open Kernel,
pass 1 in the iMode argument i.e. DspKernel(1)

- To close Kernel,
pass 0 in the iMode argument i.e. DspKernel(0)
Was this helpful?
What can we do to improve the information ?