Technical FAQs

Ask a Question

What are the different functions to export trend data to reports and databases in Vijeo Citect.

By using below functions, the trend data can be exported:
  • TrnGetTable  ->  Retrieves trend information and stores it in a Cicode array
  • TrnExportClip  ->  Copies trend data to the clipboard
  • TrnExportCSV  ->  Copies trend data to a CSV file
  • TrnExportDBF  ->  Copies trend data to a DBF file
The standard trend templates have buttons that call these functions to export data.
Was this helpful?
What can we do to improve the information ?