Technical FAQs

Ask a Question

What are the different trend storage methods in Vijeo Citect and what is difference between them.

The methods for trend data storage are:
  • Scaled method
  • Floating Point method
The Scaled is a 2-byte storage method and floating point uses 8-bytes.
Floating point storage has a dramatically expanded data range in comparison to scaled storage, allowing values to have far greater resolution. However, you need to consider that it also uses a lot more disk space.
 
Was this helpful?
What can we do to improve the information ?