Technical FAQs

Ask a Question

What is the default size of 'syslog.dat' file and how can it be increased in Vijeo Citect.

The default size of 'syslog.dat' is 2000 kb and it can be increased by '[Debug]SysLogSize' INI parameter.
For example:
This will increase the syslog.dat size to 30K kb.
Was this helpful?
What can we do to improve the information ?