Technical FAQs

Ask a Question

Can we mount Shunt trip coil and SDx Relay module simultaneously in Compact NSX MCCB's, if not what is the solution for that ?

We can not mount the Shunt trip coil and SDx module simultaneously in the Compact NSX MCCB,
If customer also want remote opening/tripping option with SDx Module then in that case customer need to use motor mechanism along with it, using the motor mechanism customer can perform closing and opening operation as well SDx module functionality (overload trip and overload pre-alarm)

Refer attachment
Was this helpful?
What can we do to improve the information ?