Technical FAQs

Ask a Question

Distance between two P54x for current differential relays.

When applying any of the P54x range of current differential relays it is important to select the appropriate protection communications interface. This will depend on the fiber used and distance between devices.
The following table attached shows the optical budgets of the available communications interfaces.
Was this helpful?
What can we do to improve the information ?