Technical FAQs

Ask a Question

In AS-B36L wiring, does the wiring configuration change for return terminal as per the input type (e.g. 4-20mA, 0-10V).

All return terminals are internally referenced to earth ground and therefore are at the same potential regardless of the input type.

Webhelp details how an extra terminal block is used on AS-B36. Refer below link for wiring configuration:
http://download.schneider-electric.com/files?p_Doc_Ref=03-18034
Was this helpful?
What can we do to improve the information ?