Technical FAQs

Ask a Question

What is surge immunity of LTMCU devices

Surge immunity According to IEC/EN 61000-4-5 is given below 

1.Line to earth/ground 1 kV (2 Ω/18 μF) level 3
2.Line to line 2 kV (2 Ω/18 μF) level 3
Was this helpful?
What can we do to improve the information ?