Technical FAQs

Ask a Question

What is the level of Immunity to electrostatic discharge of LTMCU devices.

Immunity to electrostatic discharge of LTMCU device according to  EN61000-4-2 is 8kV level 3 and 6kV level 3
Over surface.
Was this helpful?
What can we do to improve the information ?