Technical FAQs

Ask a Question

What is degree of protection as per NEMA for LTMCU

According to NEMA, degree of protection for LTMCU is Type 12 (part outside cabinet) and Type 1 (part inside cabinet)
Was this helpful?
What can we do to improve the information ?