Technical FAQs

Ask a Question

What are different functions which can be performed using Navigation keys in LTMCU

The LTM CU navigation keys are contextual, that is, their function depends on the associated icons shown on the LCD display. These icons change for different displays, so the navigation key functions also change. The navigation keys can be used to:
a)  navigate menus and sub-menus,
b) scroll within a value list,
c) select a setting in a value list,
d) exit a value list without making a selection,
e) return to the main (first-level) menu,
f) switch between manual and automatic presentation mode in Quick View display.
Was this helpful?
What can we do to improve the information ?