Technical FAQs

Ask a Question

What is the altitude derating of NSXm.


Circuit breakers are designed to operate within specification at altitudes up to 2,000 m (6,600 ft.). Above
2,000 m (6,600 ft), the following derating is required:

 
Was this helpful?
What can we do to improve the information ?