Technical FAQs

Ask a Question

In the Vijeo Citect Server-Client setup, trends are coming in Process Analyst in Server PC but not coming in Client PC even after correct configuration.

In the Server machine, all values are coming and updating in Process Analyst (or trends) but in Client machine, only a straight line is coming.
This scenario can occur when both machines have different time zones so kindly check and correct them.
After that, restart all Citect processes.

Was this helpful?
What can we do to improve the information ?