Technical FAQs

Ask a Question

What is the basic format for converting values into Strings in Vijeo Citect.

Below is the basic format of converting values into String:
In the following example, the value of a tag is converted before it is used in the DspStr() function.
Label Name
DspStr(30, "BigFont", "TEXT");
Displays "TEXT" using "BigFont" at AN30. "BigFont" needs to be defined in the Fonts database.

Note: This function is only used for V3.xx and V4.xx animations, and was superseded in later releases.

Was this helpful?
What can we do to improve the information ?