Technical FAQs

Ask a Question

Why we are getting Stop Bit Code 0x8400 (Hex) on Quantum CPU.

Stop Bit Code  0x8400 indicates that CPU has stopped because the firmware of the CRP module is not compatible with the application program in which the "Online Modification in RUN" check box has been selected .
Was this helpful?
What can we do to improve the information ?