Technical FAQs

Ask a Question

Where can the number and description of forced bits be seen in Unity Pro Project.

In a Unity Pro application, to check the number and which bits have been forced, follow the below path:
- Open PLC configuration (Double click 'PLC Bus')
- Double click Controller (CPU)
- Go to 'Animations' Tab > 'Information' Tab > Miscellaneous

Further clicking the 'FORCED BITS' will navigate to the animation table showing all the forced bits description.
Was this helpful?
What can we do to improve the information ?