Technical FAQs

Ask a Question

What are the steps which are covered by running 'Computer Setup Wizard' in a new project in Vijeo Citect.

Below are the parts of 'Computer Setup Wizard' while running a new project,
  • The role of the computer in the system network (Server, Client etc.)
  • The project that will be run
  • The CPU Configuration
  • The Events enabled for each component
  • The Cicode run for each component on startup
  • The Cluster configuration
  • The Security settings
Above steps are mandatory while running any New Project for the first time.
Was this helpful?
What can we do to improve the information ?