Technical FAQs

Ask a Question

How to set CT ratio in EM6436 ?

Press "<"(Left arrow)button from measuremnt values such as VLL, A, PF to reach "RmS".

1.After 'RmS' press "^"(Up arrow) button to reach "Clr".
2.After "Clr" press "^"(Up arrow)button to reach "Set".
3.After "Set" press ">"(Right arrow)button to reach "View".
4.After "View" press "V"(Down arrow) button to reach "Edit".
5.After "Edit" press ">"(Right arrow)button for two seconds. The display shows CODE 2000 with blinking 2.
6. Press "V"(Down arrow)button.The display shows CODE 1000 with blinking 1.
7.Press "<-"(Enter button) one time.
  The display flashes PASS and then EDIT A.PRI 100.0 indicating the successful entry to setup menu in edit mode.
8.After EDIT A.PRI 100.0, please press ">"(Right arrow)button which will result with blinking 1 (1st digit).
9.Please use "^"(Up arrow) button to increase or "V"(Down arrow) button to decrease the value as per requiremnt.
10.After that press ">"(Right arrow)button which will result with blinking 0(2nd digit) .
   Please use "^"(Up arrow) button to increase or "V"(Down arrow) button to decrease the value as per requirement.
11.Similarly press ">"(Right arrow)button which will result with blinking 0 (3rd digit).
   Please use "^"(Up arrow) button to increase or "V"(Down arrow) button to decrease the value as per requirement.
12.Similarly press ">"(Right arrow)button which will result with blinking 0 (4th digit).
   Please use "^"(Up arrow) button to increase or "V"(Down arrow) button to decrease the value as per requirement.
13.Similarly press ">"(Right arrow)button which will result with blinking "." (dot).
14.Press "<-"(Enter button) one time.
15.Press "<"(Left arrow)button then the display shows SAVE y with blinking y.
16. Press "<-"(Enter button) one time. The display flashes PASS and shows EDIT.
17. Press "<"(Left arrow)button.The display shows SET.
18. Press "V"(Down arrow)button 2 times to reach RMS.
19. press ">"(Right arrow)button to reach the measurement values.

 
Was this helpful?
What can we do to improve the information ?