Technical FAQs

Ask a Question

Which parameters are available in EM1000,EM1200 and EM1220 meter?

The following parameters are available in EM1000/EM1200 meter :-

PF PF1 PF2 PF3  Power Factor
W W1 W2 W3 /     Active Power
VA VA1 VA2 VA3 /  Volt-amperes
VAR VAR1 VAR2 VAR3 Volt-amperes reactive
KWh / KVAh / KVARh  Watt-hours / Volt-ampere hours / Volt-ampere reactive hours
Run.h  Running Hours
On.h  On hours
INTR Number of power interruptions
Was this helpful?
What can we do to improve the information ?