Technical FAQs

Ask a Question

Which MCB can be used for DC circuits with momentary current direction reversal?

iC60 MCBs can be used.

Example of DC circuits with momentary current direction reversal are given in the attached document.
Was this helpful?
What can we do to improve the information ?