Technical FAQs

Ask a Question

Are Acti9 Shunt realeases iMX continuous rated.

The Acti9 Shunt realeases iMX are continuous rated.

In fact, in all iMX devices there is a self disconnection.
That means :
- after the iMX tripped thanks to the "safety push button", the circuit of the coil of the iMX is out of voltage, automatically.
- the input of iMX can be energized all time without risk for the device.
Was this helpful?
What can we do to improve the information ?