Technical FAQs

Ask a Question

TMCR2AM3 Wiring Diagram

Wiring for TMCR2AM3. It can be done for 0-5V, 0-10V, 0-20mA and 4-20mA. Wiring for Current and Voltage input are different. Please refer the below image for more information.

 
Was this helpful?
What can we do to improve the information ?