Does the content of TSXMRPC007 memory card is retained after a cold start
TSXMRPC007 are Saved RAM memory extension cards, application + files.
The memory is saved by a removable battery built into the memory card which means it would be retained even after a cold start.