Technical FAQs

Ask a Question

To which IEC standards the G3200 offers compatibility.

The G3200 offers compatibility with:
a) IEC 61850-6 (SCL Substation Configuration Language)
b) IEC 61850-7-1 (modelling concepts)
c) IEC 61850-7-2 (ACSI Abstract Communication Service Interface)
d) IEC 61850-7-3 (common data classes)
e) IEC 61850-7-4 (Logical Nodes data and attributes)
f) IEC 61850-8-1 (mapping on Ethernet-based communication networks)
Was this helpful?
What can we do to improve the information ?