Technical FAQs

Ask a Question

What is the power supply characteristic of G3200.

The power supply characteristic of G3200 as follows:

Voltage :                        24 V DC (± 10%) supplied by a class 2 power supply
Maximum consumption:  4 W
Dielectric withstand :      1.5 kV
Was this helpful?
What can we do to improve the information ?