Technical FAQs

Ask a Question

What is the environmental characteristic of G3200.

The environmental characteristic of G3200 are as follows:

a) Operating temperature -25 °C to +70 °C (-13 °F to +158 °F)
b) Storage temperature -40 °C to +85 °C (- 40 °F to +185 °F)
c) Humidity ratio 5 to 95% relative humidity (non condensing) at +55 °C (131 °F)
d) Degree of pollution Class 2
e) Tightness IP30

 
Was this helpful?
What can we do to improve the information ?