Technical FAQs

Ask a Question

What is the overvoltage category of Powertag.

The overvoltage category of Powertag as per IEC 61010-1 is 3(III).
Was this helpful?
What can we do to improve the information ?