Technical FAQs

Ask a Question

What type of Sensors are used in B type RCCBs or RCDs ?

It is mainly because of the presence of two nonocrystalline sensors,one for the detection of Direct Current and other for the detection of default AC current of 50Hz and mixed frequencies till 1kHz.

 
Was this helpful?
What can we do to improve the information ?