Technical FAQs

Ask a Question

Is Ethernet Switch Configurator 2.2.07 Software compatible on windows 10 OS.

Yes,Ethernet Switch Configurator Version 2.2.07 can be installed on Windows 10 machine with the latest Java updates installed. It has to be started in Windows 7 compatibility mode to avoid the compatibility issue.Refer settings as in attached picture. 


 
Was this helpful?
What can we do to improve the information ?