Technical FAQs

Ask a Question

Getting error when using IP address 169.254.10.0 on BMENOC0321 module.

IP address from 169.254.0.0 to 169.254.255.255 are automatic utilized by windows when DHCP server is not active. 

(Automatic Private IP Addressing) The Windows function that provides DHCP auto configuration addressing. APIPA assigns a class B IP address from 169.254.0.0 to 169.254.255.255 to the client when a DHCP server is either permanently or temporarily unavailable. 

Hence avoid using IP addresses comes under above range. 
Was this helpful?
What can we do to improve the information ?