Technical FAQs

Ask a Question

Getting F002 error code in MBP_MSTR function block under unity Pro.

F002 indicates Component not fully initialized. This means that the module is not ready. For example after power up or cable re-connection. 
Was this helpful?
What can we do to improve the information ?