Technical FAQs

Ask a Question

What are the Port terminals used for DNP3 communication in Vamp96

Most imporant thing to understand is that for DNP3 protocol Communication there is no additional module/hardware is not required , 
it is available in Basic module only. 
Connection terminal is "X3" connector.Only the respective Firmware installed in the hardware should support the DNP3 protocol. 
The X3 connector includes two ports:Local port and Remote port.The front panel RS-232 port will shut off the local port on the rear 
panel when a VX003 cable is inserted.
For terminal connection of rear port we should use Tx Remote & Rx Remote terminal for communication, properly described in attached document.
The physical interface of this port is RS-232.
Was this helpful?
What can we do to improve the information ?