Technical FAQs

Ask a Question

What are the Input signal voltage details for IRIG- B modulated & Unmodulated in MiCOM P543

-IRIG-B 12X Interface (Modulated)
External clock synchronization per IRIG standard 200-98, format B12X.
Input impedance 6 kΩ at 1000 Hz
Modulation ratio: 3:1 to 6:1
Input signal--peak-peak: 200 mV to 20 V

- IRIG-B 00X Interface (Un-Modulated)
External clock synchronization per IRIG standard 200-98, format B00X.
Input signal-- TTL level
Input impedance at dc 10 kΩ


c
 
Was this helpful?
What can we do to improve the information ?