Technical FAQs

Ask a Question

What is the total operating time of Arc Function Self Supervision(ASF) in VAMP 321


Total operating time of ASF may vary. Operating time is dependant of teh fault type & amount of I/O units. Detection od Arc I/O 
communication timeout includes a filtering & delaying built inside ASF.

ASF - typical operating time is <1-30sec.
ASF-Arc I/O communication timeout is < 400 sec(typical: 30-180 sec)
 
Was this helpful?
What can we do to improve the information ?