Technical FAQs

Ask a Question

Which sensors are supported by VIO 12A External RTD input module.

VIO 12A modules support Pt100, Ni100, Ni120 and Cu10 type of temperature sensors
directly. For different type of thermoelements the scaling of the RTD:s can be made freely.
Was this helpful?
What can we do to improve the information ?