Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Shock & Bumps tests.

The MiCOM P14x relays conforms to Shock & Bumps tests as per IEC 60255-21-2: 1995
Shock response Class 2
Shock withstand Class 1
Bump Class 1
Was this helpful?
What can we do to improve the information ?