Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Vibration tests.

The  MiCOM P14x relays conforms to Vibration tests as per IEC 60255-21-1: 1996
Response Class 2
Endurance Class 2
Was this helpful?
What can we do to improve the information ?