Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Radiated emission tests.

The MiCOM P14x relays conforms to Radiated emission tests as per EN 55022: 1998:Class A:
30 – 230 MHz, 40 μdBV/m at 10 m measurement distance
230 – 1 GHz, 47 μdBV/m at 10 m measurement distance
Was this helpful?
What can we do to improve the information ?