Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Conducted emission tests.

The MiCOM P14x relays conforms to Conducted emission tests as per er EN 55022: 1998: Class A:
-> 0.15 - 0.5 MHz, 79 dBμV (quasi peak)
    66 dBμV (average)
-> 0.5 – 30 MHz,73 dBμV (quasi peak)
    60 dBμV (average).
Was this helpful?
What can we do to improve the information ?