Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Power Frequency Magnetic Field Immunity tests.

The MiCOM P14x relays conforms to Power Frequency Magnetic Field Immunity as

-> Per IEC 61000-4-8: 1994, Level 5,
   100 A/m applied continuously,
   1000 A/m applied for 3 s.
-> Per IEC 61000-4-9: 1993, Level 5,
   1000 A/m applied in all planes.
-> Per IEC 61000-4-10: 1993, Level 5,
   100 A/m applied in all planes at 100 kHz/1MHz with a burst duration of 2 s.
Was this helpful?
What can we do to improve the information ?