Technical FAQs

Ask a Question

Do MiCOM P14x relays conforms to Radiated Immunity from Digital Communications.

The MiCOM P14x relays conforms to Radiated Immunity from Digital Communications as per EN61000-4-3: 2002, Level 4: Test field strength, frequency band 800 to 960 MHz, and 1.4 to 2.0 GHz: 30 V/m, Test using AM: 1 kHz / 80%.
Was this helpful?
What can we do to improve the information ?